This isn’t exactly news, but if DevCon was as much of a blur for you as it was for me you may have missed the winners and very interesting runners-up in the Renesas RL78 Green Energy Challenge. You can do some really cool stuff with those RL78G13/14 RDKs sitting on the shelf in your office.

Last evening I hit the couch after dinner and picked up the latest copy of elektor, which had the full particulars, including photos, videos, diagrams, datasheets, schematics, and source code—the latter even organized as IAR projects. If any of these projects strike your fancy you can pick up where the winning entrants left off. It doesn't get easier than that.

First Prize: Electrostatic Cleaning Robot

Solar tracking mirrors, called heliostats, are an integral part of Concentrating Solar Power (CSP) plants. They must be kept clean to help maximize the production of steam, which generates power. Using an RL78, the innovative Electrostatic Cleaning Robot provides a reliable cleaning solution that’s powered entirely by photovoltaic cells. The robot traverses the surface of the mirror and uses a high voltage AC electric field to sweep away dust and debris.

Second Prize: Cloud Electrofusion Machine

Using approximately 400 times less energy than commercial electrofusion machines, the Cloud Electrofusion Machine is designed for welding 0.5″ to 2″ polyethylene fittings. The RL78-controlled machine is designed to read a barcode on the fitting which determines fusion parameters and traceability. Along with the barcode data, the system logs GPS location to an SD card, if present, and transmits the data for each fusion to a cloud database for tracking purposes and quality control.

Third Prize: The Sun Chaser: A GPS Reference Station

sss The Sun Chaser is a solar-based energy harvesting system that automatically recalculates the direction of a solar panel to ensure it is always facing the sun. Mounted on a rotating disc, the solar panel’s orientation is calculated using the registered GPS position. With an external compass, the internal accelerometer, a DC motor and stepper motor, you can determine the solar panel’s exact position. The system uses the Renesas RDKRL78G13 evaluation board running the Micrium µC/OS-III real-time kernel. 

Honorable Mentions:

Water Heater by Solar Concentration

This solar water heater is powered by the RL78 evaluation board and designed to deflect concentrated amounts of sunlight onto a water pipe for continual heating. The deflector, armed with a counterweight for easy tilting, 

Air Quality Mapper

Constructed with an RDKRL78G13, the Mapper receives location data from its GPS module, takes readings of the CO2 and CO concentrations along a specific route and stores the data in an SD card. 

High-Altitude Low-Cost Experimental Glider

Using the REFLEX flight simulator for testing, the glider has its own micro-GPS receiver, sensors and low-power MCU unit. It can take off, climb to pre-programmed altitude and return to a given coordinate.

Wireless Remote Solar-Powered “Meteo Sensor”

You can easily measure meteorological parameters with the “Meteo Sensor.” The RL78 MCU-based design takes cyclical measurements of temperature, humidity, atmospheric pressure, and supply voltage, and shares them using digital radio transceivers

Portable Power Quality Meter

The Portable Power Quality Meter uses an RL78 MCU to read power factor, total harmonic distortion, line frequency, voltage, and electrical consumption information and stores the data for analysis.