no UART Communication in UART1 in Renesas RL78G14 RDK board.

Hello,

I am using Renesas RL78G14 RDK board.

I downloaded the sample IAR project from below link:
http://in.renesas.com/support/downloads/download_results/C1000000-C9999999/tools/yrdkrl78g14_factory_demo_v39.jsp

I am unable to see UART communication in any mode supported.

I guess it looked like clocking issue.
I found multiple definition for clock freq.

/* YRDKRL78G14.h */
#define RL78_MAIN_SYSTEM_CLOCK          12000000    /* MHz */
#define RL78_SUBSYSTEM_CLOCK            32768       /* kHz */
#define RL78_INTERNAL_LOWSPEED_CLOCK    15000       /* kHz */

/* UART.c */
#define MAIN_SYSTEM_CLOCK        32000000

Could anybody confirm which value needs to be used for baud rate calculation?

Current code uses macro MAIN_SYSTEM_CLOCK

Also if any other issue is suspected in UART in RL78G14 board would really helpful

Thanks!!

regards,
Hemanth

UPDATE:

Enabling of UART-1 Tx & Rx by setting the Register "SS10", causes Higher 7 bits of the serial data register SDR02 & SDR03 to reset. How can i prevent the reset happening?