I am attempting to access the dataflash memory on an R5F100LJ by setting up a memory segment. The statement "MEMORY MY_FLASH : ( 0F1000H, 02000H )" in the linker directive file results in an error, "RA78KOR error E3116: memory area 'MY_FLASH' definition out of range". The target file used is DR5F100LJ.DVF.
Can anyone think of what must be set incorrectly?
Which compiler do you use? CA78K0R or CC-RL?
Why do you edit the linker file and do not input the section in CS+?
How do you access to the data flash? Which flash library do you use?
Thank you for responding.
I am using the CA78KOR compiler.
This code further divides the dataflash into to two segments. The CubeSuite+ manuals seem to indicate that this is accomplished by placing the following statements in the linker directive file:
MEMORY MY_FLASH : (0F1000H, 02000H)
MERGE MEM_POOL1:AT(0F1000H) = MY_FLASH
MERGE MEM_POOL2:AT(0F2000H) = MY_FLASH
Then the following pragma is required in each c file that requires access:
#pragma section @ECNSTL MEM_POOL1 /* or MEM_POOL2 */
Just out of curiousity, how is this accomplished on the Build Tools Property pages?
I will be using the pfdl.lib to write to dataflash.
Please disregard my question about how to input sections into CS+.
REGULAR 0x00000000 0x000fffff
STACK 0x000ff600 0x000ffe1f
MY_FLASH 0x000f1000 0x000f2fff
MEM_POOL1 0x000f1000 -
MEM_POOL2 0x000f2000 -
ROM 0x00000000 0x0003ffff
PFDL_COD 0x00002100 -
SEG_1 0x00038800 -
@ECNSTL 0x0000a800 -
SEG_2 0x00010000 -
RAM 0x000fb400 0x000ff5ff
RAM_SADDR 0x000ffe20 0x000fffff\
This generates the following file.
;MEMORYMEMORY STACK : ( 000ff600H, 00000820H ) / REGULARMEMORY D_FLASH : ( 000f1000H, 00002000H ) / REGULARMEMORY ROM : ( 00000000H, 00040000H ) / REGULARMEMORY RAM : ( 000fb400H, 00004200H ) / REGULARMEMORY RAM_SADDR : ( 000ffe20H, 000001e0H ) / REGULAR;SEGMENTMERGE MEM_POOL1 : AT ( 000f1000H ) = MY_FLASH / REGULARMERGE MEM_POOL2 : AT ( 000f2000H ) = MY_FLASH / REGULARMERGE PFDL_COD : AT ( 00002100H ) = ROM / REGULARMERGE SEG_1 : AT ( 00038800H ) = ROM / REGULARMERGE @ECNSTL : AT ( 0000a800H ) = ROM / REGULARMERGE SEG_2 : AT ( 00010000H ) = ROM / REGULAR
Which causes the following linker errors.
RA78KOR error E3116: Memory area 'MY_FLASH' out of range
RA78KOR error E3116: Memory area 'ROM' out of range
RA78KOR error E3210: Segment 'SEG_2' is not exist - ignored
I still have linker problems that have not been solved. Sorry, if my last message sounded as if the problem may have been solved. The end of my last shows that using the link directive generator actually increased the number of link errors. As an experiment, I commented "MEMORY ROM : ( 00000000H, 00040000H ) / REGULAR" from the generated *.dr file. Then the link errors were reduced to two:
RA78KOR error E3116: Memory area 'MY_FLASH' out of range, and
RA78KOR error E3210: Segment 'SEG_2' is not exist - ignored.
When my original *.dr file is used, only E3116 results.
Any ideas?
The segment definitions are only accepted if these sections are used in your code somewhere. Use for example for a const definition #pragma section @@CNST MemPool1
I don't know yet about E3116 because I don't have this.
And I don't why you always write ...KOR where the tools are named ...K0R.
My pragma statements are:
#pragma section @ECNSTL MEM_POOL1 // in the c file that is to access 0F1000H to 0F1FFFH, and
#pragma section @ECNSTL MEM_POOL2 // in the c file that is to access 0F2000H to 0F2FFFH
E3116 is explained as: "The sum of the start address and the size of the memory area in the memory directive is greater than 1048575(0FFFFFH)."
I do not understand. 0F1000H + 002000H < 0FFFFFH.
0 and O look very similar in CS on my screen. I will type K0R from now on.
I do have another important clue. A coworker loaded CubeSuite and my project onto his machine. The project built. We have not been able to figure out which environmental differences may be the cause.