Hello All,I am working on Renesas RL78G14 RDK.I wanted to know the maximum operating frequency the SPI(CSI) supports?I am able to configure SPI upto 2 MHz, above 2 MHz results in wrong variable clock frequency.I using the Channel-1 & Unit-3 of CSI. The system CLK(fMCK)) is set to 32 MHz.I am using the SPI as Master with clock from High-speed on-chip oscillator.Below are the register loaded values:Register Value----------------------------------------[Option byte setting]Address: 000C2H 0xF8U[Serial clock select register]SPS1 0x0000U[Transfer clock setting] SDR13 0x0200U (32 Mhz/4 = 8MHz)The SPI works fine upto 2MHz above that the clock becomes unstable.Could any share feedback regarding this issue?Thanks!!regards,Hemanth