The Renesas RX62T has long been a workhorse for motor control applications. RX63T MCUs extend those capabilities, especially in high-pin count versions.
High pin-count versions of the RX63T include more memory, connectivity options, and timers. These chips extend the RX series’ capability for motor control, with small pin-count RX63T designed for control of one motor, RX62T for two motors, and the new high pin-count…