Relocate Vector table for user application

MCU : Renesas RX111 series

Compiler : e2studio V3

Bootloader : I have a bootloader  at a Fixed ROM location and have afixed Vector Table for it.

Application : the Application have fixed ROM blocks for it..But here we need to relocate the vector table for the application as Application vector table  and Bootloader can not have same Vectortable.... 

Please suggest a solution if any....

an example will b helpful

  • e2studio V3 is NOT a compiler. It is only the IDE to control GNU, Renesas or IAR compiler.

    Define the interrupt vector table as a const table of pointers to funtions and insert the interrupt function names in this table.

    typedef void (*fp) (void);

    const fp RelocatableVectors[] = {

     (fp) function1,

     (fp) function2,

     ...

    };

    You can use the address of the array to initialise INTB.