RX111 USB interface and clock options

I am re-designing a device built around an M16C CPU, to use an RX111 to take advantage of its integrated USB interface. Now I have two doubts. The first is that I didn't find any example schematic or reference about this subject; I laid down my schematic, but I am not really sure that it is correct because I see several pins related to USB, but I connected only two (USB0_DM and USB0_DP). In the old schematic, which uses an FTDI usb-to-serial, there was at least one more connection used to reset the USB bus, and I think this would necessary too for the RX11 but I don't know how to do it.

The second doubt is about the clocking options. Is it possible to use the internal high-speed oscillator, and no external crystal, and have a working USB? I've read that the clock precision / tolerance for low speed USB is 1.5%; given that the internal high speed oscillator is rated at 1% precision, it should work - or am I missing something?

Thank you for help.

Parents Reply Children
No Data