Hello,
I would like to know if i can get some typical data about RH850/F1KM-S4 current requirement while in deep stop mode , ambient temperature say 25 degC or max 40 degC. I only want the MCU to wake up to active mode -when it receive an interrupt on a pin. The datasheet specifies a range over temperature for Deep Stop Mode current requirement.Is there any typical test data available to make an architecture design decision?
Also please let me know if i configure instead of one single pin interrupt say an additional two separate interrupt pins for wake up, will the the current draw will be more?
Thank you for the support,
Regards,
Stephen Thomas
Hi Stephen,
Sorry for the late response. Information regarding automotive products like RH850 devices are not usually shared in public so probably no one can answer your questions here in this group. But maybe Renesas Technical Support can provide you the information you're looking. Just please submit a ticket here in this page: https://en-support.renesas.com/dashboard Thank you.
JBRenesasRulz Forum Moderator
https://renesasrulz.com/https://academy.renesas.com/https://en-us.knowledgebase.renesas.com/