Hello Friends of Renses Microcontrollers
I have written a small program it was helps to calculating the CAN-Bus Bit-Timing for several microcontrollers.
Supported Renesas Controller: - RX Family - RZ Family *untested* - SuperH Family *untested* - M32R Family *untested* - M16C/R8C Family *untested* The Program is as two versions avaliable. A Windows Setup executable and as a Zip File.
Download the Windows Setup: http://www.mhs-elektronik.de/userdata/downloads/BitCalcSetup.exe
BitCalc is freeware, it comes without any warranty.Please send feedback to: [email protected]RegardsKlaus Demlehner
This thread will be archived