CAN-Bus Bit-Timing Calculator

Hello Friends of Renses Microcontrollers

I have written a small program it was helps to calculating the CAN-Bus Bit-Timing for several microcontrollers.

Supported Renesas Controller:
  - RX Family
  - RZ Family        *untested*
  - SuperH Family    *untested* 
  - M32R Family      *untested*
  - M16C/R8C Family  *untested*

The Program is as two versions avaliable. A Windows Setup executable and as a Zip File.

Download the Windows Setup: http://www.mhs-elektronik.de/userdata/downloads/BitCalcSetup.exe

BitCalc is freeware, it comes without any warranty.

Please send feedback to: [email protected]

Regards
Klaus Demlehner

BitCalc.zip
Parents Reply Children
No Data