is anyone tried to write or read from Gr-Kaede EEPROM, i am facing some problem in that, please suggest..
I am writing single byte and reading back, code work fine just after dump, now if i disconnect and connect board code is not working as intended,
it stucked somewhere in EEPROM.write() routine. Please find the code and output log below -
Sketch/Code :
#include <Arduino.h>#include "HardwareSerial.h"#include "EEPROM.h"void setup(){ unsigned char WriteByte=25,ReadByte=0; pinMode(PIN_LED0,OUTPUT); Serial.begin(9600); delay(1000); Serial.println("Writing..."); EEPROM.write(0,WriteByte); delay(500); Serial.print("you wrote : "); Serial.println(WriteByte); Serial.println("Reading..."); ReadByte = EEPROM.read(0); delay(500); Serial.print("you read :"); Serial.println(ReadByte); digitalWrite(PIN_LED0, 1);}void loop(){ //do nothing}
Output/Log :
a.)Just after code dump in the board -
Writing...you wrote : 25Reading...you read :25
b.) After disconnect and reconnect board (Power off-on) :
Writing...