Problem with Camera. Does anyone connected camera without camera shield?

Hi,

I have the requirement to use camera (without directly mounting on to GR Kaede board) with 24 wires connected to GR Kaede board. The max length of wire I used is 30 cm's. I am not able to figure out which pins are used by camera and which are available free for different use on the GR Kaede board. If there is any pin layout diagram between camera and GR Kaede board, please share. My requirement is simple, i have to take a pic at regular intervals and store in the SD card. If anybody have a sample code, please share. Thank you.

Parents Reply Children
No Data