I developed a product that is based on RL78/G13's 20 pin IC, now when I program it using GR KURUMI' IDE I received an error saying "Read failed" but it detects my boardwhat could be the reason behind it? is there any need for configuration that needs to be done?I have already replicated GR KURUMI's board and developed my own using 52pin RL78/G13 which was successful.
Error:
F:\REN_ide4gr-1.13-windows_SWR_20200902\ide4gr-1.13/hardware/tools/gcc-rl78/rl78-elf/rl78-elf/lib\libstdc++.a(pure.o): In function `__cxa_pure_virtual':(.text.__cxa_pure_virtual+0x12): warning: _write is not implemented and will always failBinary sketch size: 22,090 bytes (of a 262,144 byte maximum) - 8% usedMinimum Memory usage: 2,648 bytes (of a 20,480 byte maximum) - 12% usedDevice: R5F1006C Code size: 32 kBData size: 4 kBErasecygwin warning: MS-DOS style path detected: C:\Users\KOVARD~1\AppData\Local\Temp\build5485136465074631415.tmp/Blink.cpp.mot Preferred POSIX equivalent is: /cygdrive/c/Users/KOVARD~1/AppData/Local/Temp/build5485136465074631415.tmp/Blink.cpp.mot CYGWIN environment variable option "nodosfilewarning" turns off this warning. Consult the user's guide for more details about POSIX paths: cygwin.com/.../using.htmlRead failed................................Read file "C:\Users\KOVARD~1\AppData\Local\Temp\build5485136465074631415.tmp/Blink.cpp.mot"
This looks to not be a device related question, but a tool question. Perhaps the more appropriate forum for this would be the GR-KRUMI forum:
https://renesasrulz.com/gadget_renesas_user_forum/f/gr-kurumi---forum--