Hi all
How to short JP3/JP4 ? There is no exposed jumper connector, so do we need to permanently solder ?
I want to use I2C lines for communicating sensor data to the Controller.
So, How to short JP3/JP4 ? Is it permanently to be soldered or any idea of shorting it when required ?
Also ,
Unable to
located R43/R45 on board which says two.seven k ohm, Is it internally pulled up or
should i use the same value resistors for external pull up ?
Thanks,
sbw