I2C pull up- GR Lychee

Hi all

Jumper connections

How to short JP3/JP4 ? There is no exposed jumper connector, so do we need to permanently solder ? 

I want to use I2C lines for communicating sensor data to the Controller.

 

So, How to short JP3/JP4 ? Is it permanently to be soldered or any idea of shorting it when required ?

Also ,

Pullups

Unable to

located R43/R45 on board which says two.seven k ohm, Is it internally pulled up or 

should i use the same value resistors for external pull up ?

 

Thanks,

sbw