How to access GR-PEACH as web camera.

HI,
I am working with GR-PEACH version F(X28A-M01F).Any one tell how to set ip address for board in program using IDE and also please send the sample code and library to be used.
thank you.

  • In case of using IDE for GR(Arduino sketch), the sample for web camera exist like below.

    // Sample for GR-PEACH
    //
    // Required hardware: Ethernet, following files stored in SD
    // index.htm : gadget.renesas.com/.../index.htm
    //
    // Public Domain

    #include <Arduino.h>
    #include "SPI.h"
    #include "SD.h"
    #include "HTTPServer.h"
    #include "EthernetInterface.h"
    #include "FATFileSystem.h"
    #include "RomRamBlockDevice.h"
    #include "Camera.h"

    FATFileSystem fs("storage");
    RomRamBlockDevice romram_bd(512000, 512);
    #define NUM_WEBFILES 1
    const char mount_files[NUM_WEBFILES][13] = { //name should be 8.3 format
    "index.htm"};

    /** Network setting **/
    // #define IP_ADDRESS ("192.168.11.2") /* IP address */
    // #define SUBNET_MASK ("255.255.255.0") /* Subnet mask */
    // #define DEFAULT_GATEWAY ("192.168.11.3") /* Default gateway */

    Camera camera(640, 480);
    EthernetInterface network;
    File myFile;

    static int snapshot_req(const char ** pp_data) {

    int encode_size = camera.createJpeg();
    *pp_data = (const char *) camera.getJpegAdr();
    ;
    return encode_size;
    }

    static void mount_romramfs(void) {
    FILE * fp;

    romram_bd.SetRomAddr(0x18000000, 0x1FFFFFFF);
    fs.format(&romram_bd, 512);
    fs.mount(&romram_bd);

    char write_path[20];

    for (int i = 0; i < NUM_WEBFILES; i++) {
    myFile = SD.open(mount_files[i], FILE_READ);
    if (myFile) {
    sprintf(write_path, "/storage/%s", mount_files[i]);
    fp = fopen(write_path, "w");
    // read from the file until there's nothing else in it:
    while (myFile.available()) {
    putc(myFile.read(), fp);
    }
    // close the file:
    myFile.close();
    fclose(fp);
    }
    }
    }

    void setup(void) {

    Serial.begin(9600);
    Serial.print("********* PROGRAM START ***********\r\n");

    if (!SD.begin()) {
    return;
    }

    mount_romramfs(); //RomRamFileSystem Mount
    camera.begin();

    if (network.connect() != 0) {
    return;
    }

    Serial.print("MAC Address is ");
    Serial.println(network.get_mac_address());
    Serial.print("IP Address is ");
    Serial.println(network.get_ip_address());
    Serial.print("NetMask is ");
    Serial.println(network.get_netmask());
    Serial.print("Gateway Address is ");
    Serial.println(network.get_gateway());
    Serial.println("Network Setup OK\r\n");

    SnapshotHandler::attach_req(&snapshot_req);
    FSHandler::mount("/storage", "/");
    HTTPServerAddHandler<SnapshotHandler>("/camera"); //Camera
    HTTPServerAddHandler<FSHandler>("/");
    HTTPServerStart(&network, 80);

    }

    void loop() {
    }