GR-Rose in USB Host Configuration

Hello GR-Rose team,

Can we use GR-Rose in USB Host configuration?

If so, do we need to do any hardware modifications?

Regards,

Kamal 

Parents
  • Hi Kamal,

    You need to supply 5V to an external device. Make sure the terminal "USB0_VBUSEN" "USB0_OVRCURA" are not connected to RX65N on GR-ROSE, so you should take care the functions on these terminals are not available, for example the detection of over current.
  • Hello Yuuki-san,

    Thank you for the response on this topic.

    We have confirmed that these pins are not assigned as USB pins in the MPC configuration.
    We have connected USB Y-cable to PC, GR-Rose and USB memory stick. PC is providing the 5V supply to both GR-Rose and Memory stick.

    With this configuration, USB connection is not working.
    Observation: Upon connection of USB memory stick to Y-cable, RX-65N receives attach interrupt but after that, there are no transaction seen on the bus when checked with a USB analyzer.

    However, we have confirmed that USB host configuration is working fine with RSK-2MB board.
    Any information on this would be really helpful?

    Regards,
    Kamal
Reply
  • Hello Yuuki-san,

    Thank you for the response on this topic.

    We have confirmed that these pins are not assigned as USB pins in the MPC configuration.
    We have connected USB Y-cable to PC, GR-Rose and USB memory stick. PC is providing the 5V supply to both GR-Rose and Memory stick.

    With this configuration, USB connection is not working.
    Observation: Upon connection of USB memory stick to Y-cable, RX-65N receives attach interrupt but after that, there are no transaction seen on the bus when checked with a USB analyzer.

    However, we have confirmed that USB host configuration is working fine with RSK-2MB board.
    Any information on this would be really helpful?

    Regards,
    Kamal
Children