Example projects won't compile - i.e BarometricPressureSensor

Hi 

I tried to compile BarometriPressureSensor example project on GR Ide 1.13 (also tried older versions).

It shows multiple problems, possibly with SPI library and iodefine

Also checked SPI on web compiler and similar problems appeared.

 

Board: GR-Sakura

 

I am trying to run UbidotsEthernet on GR-Sakura but as mentioned basic spi libraries have problems.

Parents
  • Hi, I'm Okamiya in Gadget Renesas.

    I tried compiling the below code as described in the following web site. There is no problem with that. Can you tell me which code you tried.

    www.arduino.cc/.../BarometricPressureSensor

     

    #include <SPI.h>
    //Sensor&apos;s memory register addresses:
    const int PRESSURE = 0x1F; //3 most significant bits of pressure
    const int PRESSURE_LSB = 0x20; //16 least significant bits of pressure
    const int TEMPERATURE = 0x21; //16 bit temperature reading
    const byte READ = 0b11111100; // SCP1000&apos;s read command
    const byte WRITE = 0b00000010; // SCP1000&apos;s write command
    // pins used for the connection with the sensor
    // the other you need are controlled by the SPI library):
    const int dataReadyPin = 6;
    const int chipSelectPin = 7;
    void setup() {
    Serial.begin(9600);
    // start the SPI library:
    SPI.begin();
    // initalize the data ready and chip select pins:
    pinMode(dataReadyPin, INPUT);
    pinMode(chipSelectPin, OUTPUT);
    //Configure SCP1000 for low noise configuration:
    writeRegister(0x02, 0x2D);
    writeRegister(0x01, 0x03);
    writeRegister(0x03, 0x02);
    // give the sensor time to set up:
    delay(100);
    }

    void loop() {
    //Select High Resolution Mode
    writeRegister(0x03, 0x0A);
    // don&apos;t do anything until the data ready pin is high:
    if (digitalRead(dataReadyPin) == HIGH) {
    //Read the temperature data
    int tempData = readRegister(0x21, 2);
    // convert the temperature to celsius and display it:
    float realTemp = (float)tempData / 20.0;
    Serial.print("Temp[C]=");
    Serial.print(realTemp);
    //Read the pressure data highest 3 bits:
    byte pressure_data_high = readRegister(0x1F, 1);
    pressure_data_high &= 0b00000111; //you only needs bits 2 to 0
    //Read the pressure data lower 16 bits:
    unsigned int pressure_data_low = readRegister(0x20, 2);
    //combine the two parts into one 19-bit number:
    long pressure = ((pressure_data_high << 16) | pressure_data_low) / 4;
    // display the temperature:
    Serial.println("\tPressure [Pa]=" + String(pressure));
    }
    }

    //Read from or write to register from the SCP1000:
    unsigned int readRegister(byte thisRegister, int bytesToRead) {
    byte inByte = 0; // incoming byte from the SPI
    unsigned int result = 0; // result to return
    Serial.print(thisRegister, BIN);
    Serial.print("\t");
    // SCP1000 expects the register name in the upper 6 bits
    // of the byte. So shift the bits left by two bits:
    thisRegister = thisRegister << 2;
    // now combine the address and the command into one byte
    byte dataToSend = thisRegister & READ;
    Serial.println(thisRegister, BIN);
    // take the chip select low to select the device:
    digitalWrite(chipSelectPin, LOW);
    // send the device the register you want to read:
    SPI.transfer(dataToSend);
    // send a value of 0 to read the first byte returned:
    result = SPI.transfer(0x00);
    // decrement the number of bytes left to read:
    bytesToRead--;
    // if you still have another byte to read:
    if (bytesToRead > 0) {
    // shift the first byte left, then get the second byte:
    result = result << 8;
    inByte = SPI.transfer(0x00);
    // combine the byte you just got with the previous one:
    result = result | inByte;
    // decrement the number of bytes left to read:
    bytesToRead--;
    }
    // take the chip select high to de-select:
    digitalWrite(chipSelectPin, HIGH);
    // return the result:
    return (result);
    }

    //Sends a write command to SCP1000

    void writeRegister(byte thisRegister, byte thisValue) {
    // SCP1000 expects the register address in the upper 6 bits
    // of the byte. So shift the bits left by two bits:
    thisRegister = thisRegister << 2;
    // now combine the register address and the command into one byte:
    byte dataToSend = thisRegister | WRITE;
    // take the chip select low to select the device:
    digitalWrite(chipSelectPin, LOW);
    SPI.transfer(dataToSend); //Send register location
    SPI.transfer(thisValue); //Send value to record into register
    // take the chip select high to de-select:
    digitalWrite(chipSelectPin, HIGH);
    }

Reply
  • Hi, I'm Okamiya in Gadget Renesas.

    I tried compiling the below code as described in the following web site. There is no problem with that. Can you tell me which code you tried.

    www.arduino.cc/.../BarometricPressureSensor

     

    #include <SPI.h>
    //Sensor&apos;s memory register addresses:
    const int PRESSURE = 0x1F; //3 most significant bits of pressure
    const int PRESSURE_LSB = 0x20; //16 least significant bits of pressure
    const int TEMPERATURE = 0x21; //16 bit temperature reading
    const byte READ = 0b11111100; // SCP1000&apos;s read command
    const byte WRITE = 0b00000010; // SCP1000&apos;s write command
    // pins used for the connection with the sensor
    // the other you need are controlled by the SPI library):
    const int dataReadyPin = 6;
    const int chipSelectPin = 7;
    void setup() {
    Serial.begin(9600);
    // start the SPI library:
    SPI.begin();
    // initalize the data ready and chip select pins:
    pinMode(dataReadyPin, INPUT);
    pinMode(chipSelectPin, OUTPUT);
    //Configure SCP1000 for low noise configuration:
    writeRegister(0x02, 0x2D);
    writeRegister(0x01, 0x03);
    writeRegister(0x03, 0x02);
    // give the sensor time to set up:
    delay(100);
    }

    void loop() {
    //Select High Resolution Mode
    writeRegister(0x03, 0x0A);
    // don&apos;t do anything until the data ready pin is high:
    if (digitalRead(dataReadyPin) == HIGH) {
    //Read the temperature data
    int tempData = readRegister(0x21, 2);
    // convert the temperature to celsius and display it:
    float realTemp = (float)tempData / 20.0;
    Serial.print("Temp[C]=");
    Serial.print(realTemp);
    //Read the pressure data highest 3 bits:
    byte pressure_data_high = readRegister(0x1F, 1);
    pressure_data_high &= 0b00000111; //you only needs bits 2 to 0
    //Read the pressure data lower 16 bits:
    unsigned int pressure_data_low = readRegister(0x20, 2);
    //combine the two parts into one 19-bit number:
    long pressure = ((pressure_data_high << 16) | pressure_data_low) / 4;
    // display the temperature:
    Serial.println("\tPressure [Pa]=" + String(pressure));
    }
    }

    //Read from or write to register from the SCP1000:
    unsigned int readRegister(byte thisRegister, int bytesToRead) {
    byte inByte = 0; // incoming byte from the SPI
    unsigned int result = 0; // result to return
    Serial.print(thisRegister, BIN);
    Serial.print("\t");
    // SCP1000 expects the register name in the upper 6 bits
    // of the byte. So shift the bits left by two bits:
    thisRegister = thisRegister << 2;
    // now combine the address and the command into one byte
    byte dataToSend = thisRegister & READ;
    Serial.println(thisRegister, BIN);
    // take the chip select low to select the device:
    digitalWrite(chipSelectPin, LOW);
    // send the device the register you want to read:
    SPI.transfer(dataToSend);
    // send a value of 0 to read the first byte returned:
    result = SPI.transfer(0x00);
    // decrement the number of bytes left to read:
    bytesToRead--;
    // if you still have another byte to read:
    if (bytesToRead > 0) {
    // shift the first byte left, then get the second byte:
    result = result << 8;
    inByte = SPI.transfer(0x00);
    // combine the byte you just got with the previous one:
    result = result | inByte;
    // decrement the number of bytes left to read:
    bytesToRead--;
    }
    // take the chip select high to de-select:
    digitalWrite(chipSelectPin, HIGH);
    // return the result:
    return (result);
    }

    //Sends a write command to SCP1000

    void writeRegister(byte thisRegister, byte thisValue) {
    // SCP1000 expects the register address in the upper 6 bits
    // of the byte. So shift the bits left by two bits:
    thisRegister = thisRegister << 2;
    // now combine the register address and the command into one byte:
    byte dataToSend = thisRegister | WRITE;
    // take the chip select low to select the device:
    digitalWrite(chipSelectPin, LOW);
    SPI.transfer(dataToSend); //Send register location
    SPI.transfer(thisValue); //Send value to record into register
    // take the chip select high to de-select:
    digitalWrite(chipSelectPin, HIGH);
    }

Children
No Data