Hi guys, when i had compile the coding below which is from the ide itsel to the sakura board , it does not shows anything on the serial monitor . Does anyone know what is the problem?
/* AnalogReadSerial Reads an analog input on pin 0, prints the result to the serial monitor. Attach the center pin of a potentiometer to pin A0, and the outside pins to +3.3V and ground. This example code is in the public domain. */
// the setup routine runs once when you press reset:void setup() { // initialize serial communication at 9600 bits per second: Serial.begin(9600);}
// the loop routine runs over and over again forever:void loop() { // read the input on analog pin 0: int sensorValue = analogRead(A0); // print out the value you read: Serial.println(sensorValue); delay(1); // delay in between reads for stability}
Hi wan,
Did you check if you've selected the right COM port? Also, what is that error message on the image you've attached?
JBIf this response, or one provided by another user, answers your question, please verify the answer. Thank you!RenesasRulz Forum Moderatorhttps://renesasrulz.com/https://academy.renesas.com/https://en-support.renesas.com/knowledgeBase/
hi JB,i had found the issue and resolved it . The error message on the image are warning _ write is not implemented and will always fail.
Thanks.
Wan