Hi guys, when i had compile the coding below which is from the ide itsel to the sakura board , it does not shows anything on the serial monitor . Does anyone know what is the problem?
/* AnalogReadSerial Reads an analog input on pin 0, prints the result to the serial monitor. Attach the center pin of a potentiometer to pin A0, and the outside pins to +3.3V and ground. This example code is in the public domain. */
// the setup routine runs once when you press reset:void setup() { // initialize serial communication at 9600 bits per second: Serial.begin(9600);}
// the loop routine runs over and over again forever:void loop() { // read the input on analog pin 0: int sensorValue = analogRead(A0); // print out the value you read: Serial.println(sensorValue); delay(1); // delay in between reads for stability}