Sample Codes for Kurumi Eye Shield

Original: http://japan.renesasrulz.com/gr_user_forum_japanese/m/mediagallery/141.aspx

By: Yuuki Okamiya

This is a demo program for Kurumi Eye Shield with Xbee. The program transmit 16-bit ID, temperature, luminescence, and X-Y-Z acceleration values in orders via XBee serial.  And then GR-SAKURA receives the data and prints on COM screen.  The attached ZIP codes is for GR-SAKURA.

You can download the XBee library from here:

https://code.google.com/p/xbee-arduino/

sakura_xbee_library.zip