Ethernet server not working :: need help on it

Hi,

I have written a ethernet server based on the code found in net.

Sakura is not responding for the ethernet frames from client. I am using offline compiler

Code ::

#include <rxduino.h>
#include <Ethernet.h>

#define INTERVAL 100
byte mac[] = {0x08, 0x09, 0x3c, 0x12, 0x34, 0x56};
byte ip[] = {192,168,0,2};

TEthernet Ethernet;
EthernetServer server (80);
void setup()
{
    pinMode(PIN_LED0,OUTPUT);
    pinMode(PIN_LED1,OUTPUT);
    pinMode(PIN_LED2,OUTPUT);
    pinMode(PIN_LED3,OUTPUT);
    Serial.begin(115200,SCI_SCI0P2x);
    
    Ethernet.begin(mac,ip);
        Serial.write("Ethernet done \n");
Serial.print("My IP address is: ");

   Serial.println(Ethernet.localIP());        
    server.begin();
        Serial.write("Server begin done \n");
        
/*
speed: Baud rate
The port: port to be used (if omitted, use the virtual COM port of USB0)
I use a virtual COM port USB0: SCI_USB0
I use the (TxD) (RxD), pin 30 pin 31 SCI_SCI2A
I use the (RxD) (TxD), pin 26 SCI_SCI2B pin 24. Used to access XBee
I use the (RxD) (TxD), Pin 6 Pin 7 SCI_SCI6B
I use the (TxD) (RxD), pin 1 SCI_SCI0P2x pin 0
Select the one it received for the first time in USB0 or SCI_AUTO pin 0,1
*/
Serial.write("Setup done \n");
}

void loop()
{
EthernetClient client;
    client = server.available ();
    




    if (client) {  // got client?
        boolean currentLineIsBlank = true;
    digitalWrite(PIN_LED0, 1);
    delay(INTERVAL);
            while (client.connected()) {
                digitalWrite(PIN_LED1, 1);
    delay(INTERVAL);

            if (client.available()) {   // client data available to read
                char c = client.read(); // read 1 byte (character) from client
                // last line of client request is blank and ends with \n
                // respond to client only after last line received
    digitalWrite(PIN_LED2, 1);
    delay(INTERVAL);
                    if (c == '\n' && currentLineIsBlank) {
    digitalWrite(PIN_LED3, 1);
    delay(INTERVAL);
                        // send a standard http response header
                    client.println("HTTP/1.1 200 OK");
                    client.println("Content-Type: text/html");
                    client.println("Connection: close");
                    client.println();
                    // send web page
                    client.println("<!DOCTYPE html>");
                    client.println("<html>");
                    client.println("<head>");
                    client.println("<title>GK-Sakura Web Page</title>");
                    client.println("</head>");
                    client.println("<body>");
                    client.println("<h1>Hello from GK-Sakura!</h1>");
                    client.println("<p>A web page from the GK-Sakura server</p>");
                    client.println("</body>");
                    client.println("</html>");
                    break;
                }
                // every line of text received from the client ends with \r\n
                if (c == '\n') {
                    // last character on line of received text
                    // starting new line with next character read
                    currentLineIsBlank = true;
                }
                else if (c != '\r') {
                    // a text character was received from client
                    currentLineIsBlank = false;
                }
            } // end if (client.available())
        } // end while (client.connected())
        delay(1);      // give the web browser time to receive the data
        client.stop(); // close the connection
    } // end if (client)
//    Serial.write("LOOP\n");
}

Parents
  • Hi I cant really help with the software side, but just a few thoughts

    It would be useful to explain how you are using the Ethernet interface without having to look through all the code

    This would help someone to understand in more detail the problem and for the users who are using the Ethernet interface see if it is similar to your design

    Make sure that if you are using the internal hardware Ethernet and PHY that all the connections, jumpers and interfaces etc. are set correctly (especially if you have been using the board for any other functions)

    Also that if you are porting code from the web many Arduino Ethernet implementations use an external shield board to provide the MAC and PHY and a serial interface between the MCU and the shield board

    (often SPI as this is the fastest). The Ethernet interface on the GR-Sakuara board I am sure you are aware is connected directly to the RX63N MCU

    Also there a number of posts in the forum and India design contexts about using Ethernet, which may be of some assistance with your problem

    Sorry I can't be of more help

  • Hi,

    I too tried this out, and it didnt work out at all ... Been on it for a while now. Have you gotten it to work / any progress at all ?

  • Hi AbdealiJK,

    Is my code posted in the forum is not working for you. or any code for ethernet is not working for you.

    I doubt it might be hw problem. I have taken the code from internet only, they placed it with working code only. I suspect the hw.

  • I did try your code out, but didnt debug properly(didnt have time) ... was planning on doing it tomorrow.

    I did try out some other codes online and also went through a website which had explanations of each function in Ethrnet library and made my code. That too did not work.

    I the latter approach had some issues with the dhcp itself (i think) ... as ...

    When i gave it a static IP in the ethernet.begin function, it continued past the Ethernet.begin function, but My laptop could not find the ip in it's local group...

  • I also answered to another user in another blog that there are many reasons, what could be wrong (e.g. router setup, MAC filtering, wrong IP range, etc.), see: renesasrulz.com/.../3839.aspx

    And I also have posted there that I also have difficulties to get the Ethernet web server running with the OFFline compiler. So, please try that first using the ONline web compiler.

    Anyway, here's my code, which definitely works. It worked with using the DHCP (without using the ip address) and using the ip setting manually. Honestly speaking, I'm not sure which impact the MAC address has. But mine is different. I think, it shouldn't matter (unless you have a MAC filtering in your router enabled, which might block certain MAC addresses).

    Here's my code:

    #define RXDUINO

    // increase compatibility to test also for Arduino

    #ifdef RXDUINO

    #include <rxduino.h>

    #else

    #include <Arduino.h>

    #include <SPI.h>

    #endif

    #include <Ethernet.h>

    #ifdef RXDUINO

    TEthernet Ethernet;

    #endif

    // MAC-Adresse

    byte mac[] = {

       0x90, 0xA2, 0xDA, 0x0D, 0x02, 0x8C};  // ensure it's not blocked by router or network

    byte ip[] = {

       0xC0, 0xA8, 0x02, 0x69};  // not used, but can be used...

    EthernetServer server(80);

    const int analogPin = A0;

    const int inputTestPin = 0;

    const int led1 = 1;

    const int led2 = 2;

    void setup()

    {

     pinMode(PIN_LED0,OUTPUT);          // for debugging

     pinMode(PIN_LED3,OUTPUT);          // for debugging

     pinMode(inputTestPin, INPUT);      // for testing

     digitalWrite(PIN_LED0, LOW);

     digitalWrite(PIN_LED3, LOW);

     pinMode(led1,OUTPUT);         // for debugging

     pinMode(led2,OUTPUT);

     digitalWrite(led1,0);          

     digitalWrite(led2,0);          

     Serial.begin(9600); // Bit rate don't care if via USB

     delay(500);

       // use ONLY that statement if ip is fixed:

       //      Ethernet.begin(mac, ip);

       // if DHCP, no further variable necessary, but check for getting IP correctly

       if (Ethernet.begin(mac) == 0) {

            Serial.println("Failed get address on DHCP");

           while(1);  // loop forever in case of error = stop

       }

       Serial.println("Get IP address from DHCP is success.");

       server.begin();

       Serial.print("Please access by browser at http://");

       Serial.println(Ethernet.localIP());

    }

    char outStr[80];

    void loop()

    {

       EthernetClient client = server.available();

       if (client) {

           Serial.println("new client");

           boolean currentLineIsBlank = true;

           while (client.connected()) {

    #ifdef RXDUINO

               Ethernet.processPackets();

    #endif      

               if (client.available()) {

                   digitalWrite(PIN_LED0, HIGH);   // Server ist UP!

                   char c = client.read();

                   Serial.write(c);

                   if (c == '\n' && currentLineIsBlank) {

                       digitalWrite(PIN_LED3, HIGH);   // shows: client request is there

                       // http

                       client.println("HTTP/1.1 200 OK");

                       client.println("Content-Type: text/html");

                       client.println("Connection: close");

                       client.println();

                       client.println("<!DOCUTYPE HTML>");

                       client.println("<html>");

                       client.println("<h1>Answer from GR-Sakura</h1><p style='color:red; font-weight:bold;'>Hello!</p>");

                       sprintf( outStr , "Value of Analog Pin A0: %d value of Digital Pin 0: %d  LED1 is: %d", analogRead(analogPin), digitalRead(inputTestPin), digitalRead(led1) );

                       client.println(outStr);

                       client.println("</html>");

                       break;

                   }

                   // EOL(\n)

                   if (c == '\n') {

                       currentLineIsBlank = true;

                   }

                   //

                   else if (c != '\r') {

                       currentLineIsBlank = false;

                   }

               }

           }

           delay(10);

           client.stop();

    //       digitalWrite(PIN_LED0, LOW);   // Server ist DOWN!

           Serial.println("client disconnected");

       }      

    }

    (if it helps, I also could post the sketch.bin file)

  • I have tried both offline and online compilers, it is not working for me.i will try your code. Are usingUSB as serial connection. I tried to install driver, somehow, devices is not detecting as com  port.

  • seems you have a basic problem.

    I'm not sure which OS you are using, but for Windows maybe this thread might help:

    renesasrulz.com/.../508.aspx

    or that with some additional explanations:

    renesasrulz.com/.../3779.aspx

    Sometimes, I made the experience that the USB serial port and connection to the USB terminal does not work immediately after uploading the code. So, try to remove the USB connection after uploading the sketch.bin and connect it again and try again then to connect via the USB terminal.

Reply Children