GR-SAKURA is not found.

Hello all,

I have received my GR-SAKURA and I have loaded the LED demo via the web compiler just fine. The problem I am having is that the offline IDE is not finding my board when I hit reset and put it into flash drive mode. I have tried version 0.7.0 and version 0.8.0 and both have the same issue.

Does anyone know if the GR-SAKURA is fully supported yet?

Thanks,

James

Parents Reply Children
  • Solved my problem.

    It is a problem in version 0.8.0 and version 0.7.0 of the ide4gr and yes I grabbed it from the hyperlink you supplied.

    In the file ide4gr\hardware\tools\rx\CheckVolume.bat line 7 has "tokens=5". Changing this to be "tokens=6" fixes the script and is now runs fine.

    The problem was the script was setting the VOLNAME="is".

       D:\Sakura\ide4gr-E0.8.0\hardware\tools\rx>CheckVolume.bat I GR-SAKURA

       D:\Sakura\ide4gr-E0.8.0\hardware\tools\rx>rem ÄwÆΦé╡é╜â{âèâàü[âÇé¬ÄwÆΦé╡é╜û╝æOé╞êΩÆvé╖éΘé⌐â`âFâbâNé╖éΘâoâbâ`âtâ@âCâï

       D:\Sakura\ide4gr-E0.8.0\hardware\tools\rx>rem I èmöFé╖éΘâ{âèâàü[âÇû╝üiâAâïâtâ@âxâbâgüj

       D:\Sakura\ide4gr-E0.8.0\hardware\tools\rx>rem GR-SAKURA îƒì⌡é╖éΘâ{âèâàü[âÇû╝üiGR-?üj

       D:\Sakura\ide4gr-E0.8.0\hardware\tools\rx>set VOLNAME=0

       D:\Sakura\ide4gr-E0.8.0\hardware\tools\rx>for /F "tokens=5" %v in ('vol I:') do set VOLNAME=%v

       D:\Sakura\ide4gr-E0.8.0\hardware\tools\rx>set VOLNAME=is

       D:\Sakura\ide4gr-E0.8.0\hardware\tools\rx>set VOLNAME=0000-0000

       D:\Sakura\ide4gr-E0.8.0\hardware\tools\rx>if "0000-0000" == "GR-SAKURA" (exit /b 0 )

       D:\Sakura\ide4gr-E0.8.0\hardware\tools\rx>exit /b 1

    the output of  command "vol i:":

       D:\Sakura\ide4gr-E0.8.0\hardware\tools\rx>vol I:

        Volume in drive I is GR-SAKURA

        Volume Serial Number is 0000-0000

    so you can see that it was off by one token, therefore I set the value to be 6 and the out put of the script is:

       D:\Sakura\ide4gr-E0.8.0\hardware\tools\rx>CheckVolume.bat I GR-SAKURA

       D:\Sakura\ide4gr-E0.8.0\hardware\tools\rx>rem ÄwÆΦé╡é╜â{âèâàü[âÇé¬ÄwÆΦé╡é╜û╝æOé╞êΩÆvé╖éΘé⌐â`âFâbâNé╖éΘâoâbâ`âtâ@âCâï

       D:\Sakura\ide4gr-E0.8.0\hardware\tools\rx>rem I èmöFé╖éΘâ{âèâàü[âÇû╝üiâAâïâtâ@âxâbâgüj

       D:\Sakura\ide4gr-E0.8.0\hardware\tools\rx>rem GR-SAKURA îƒì⌡é╖éΘâ{âèâàü[âÇû╝üiGR-?üj

       D:\Sakura\ide4gr-E0.8.0\hardware\tools\rx>set VOLNAME=0

       D:\Sakura\ide4gr-E0.8.0\hardware\tools\rx>for /F "tokens=6" %v in ('vol I:') do set VOLNAME=%v

       D:\Sakura\ide4gr-E0.8.0\hardware\tools\rx>set VOLNAME=GR-SAKURA

       D:\Sakura\ide4gr-E0.8.0\hardware\tools\rx>if "GR-SAKURA" == "GR-SAKURA" (exit /b 0 )

    Hope this helps people in the future......

    James

  • Hi James !
    I have also this problem of "GR-SAKURA not found" :(
    I have done what you did : tokens=5 to tokens=6
    but I still have the same issue : when I want to download my bin from IDE for GR (0.8.0) it says GR-SAKURA is not found.
    Could you help me ...
    My OS is windows 10
    Thanks
  • Hello James, I did like you said. Changed the .bat file and replace "tokens=5" to "tokens=6" but i have the same trouble.
    Everytime i want to upload the file into the Sakura, IDE shows me a message "GR-SAKURA not found"


    Can you tell me more in detail what you did and from where you got that script that tells how it's working. This is what i have from IDE's log

    C:\Users\Lourdes\Downloads\ide4gr-1.10-windows\ide4gr-1.10/hardware/tools/gcc-rx/rx-elf/rx-elf/rx-elf/lib/64-bit-double\libc.a(lib_a-closer.o): In function `_close_r':
    (.text._close_r+0x10): warning: _close is not implemented and will always fail
    C:\Users\Lourdes\Downloads\ide4gr-1.10-windows\ide4gr-1.10/hardware/tools/gcc-rx/rx-elf/rx-elf/rx-elf/lib/64-bit-double\libc.a(lib_a-fstatr.o): In function `_fstat_r':
    (.text._fstat_r+0x12): warning: _fstat is not implemented and will always fail
    C:\Users\Lourdes\Downloads\ide4gr-1.10-windows\ide4gr-1.10/hardware/tools/gcc-rx/rx-elf/rx-elf/rx-elf/lib/64-bit-double\libc.a(lib_a-signalr.o): In function `_getpid_r':
    (.text._getpid_r+0x1): warning: _getpid is not implemented and will always fail
    C:\Users\Lourdes\Downloads\ide4gr-1.10-windows\ide4gr-1.10/hardware/tools/gcc-rx/rx-elf/rx-elf/rx-elf/lib/64-bit-double\libc.a(lib_a-isattyr.o): In function `_isatty_r':
    (.text._isatty_r+0x10): warning: _isatty is not implemented and will always fail
    C:\Users\Lourdes\Downloads\ide4gr-1.10-windows\ide4gr-1.10/hardware/tools/gcc-rx/rx-elf/rx-elf/rx-elf/lib/64-bit-double\libc.a(lib_a-signalr.o): In function `_kill_r':
    (.text._kill_r+0x12): warning: _kill is not implemented and will always fail
    C:\Users\Lourdes\Downloads\ide4gr-1.10-windows\ide4gr-1.10/hardware/tools/gcc-rx/rx-elf/rx-elf/rx-elf/lib/64-bit-double\libc.a(lib_a-lseekr.o): In function `_lseek_r':
    (.text._lseek_r+0x14): warning: _lseek is not implemented and will always fail
    C:\Users\Lourdes\Downloads\ide4gr-1.10-windows\ide4gr-1.10/hardware/tools/gcc-rx/rx-elf/rx-elf/rx-elf/lib/64-bit-double\libc.a(lib_a-readr.o): In function `_read_r':
    (.text._read_r+0x14): warning: _read is not implemented and will always fail
    C:\Users\Lourdes\Downloads\ide4gr-1.10-windows\ide4gr-1.10/hardware/tools/gcc-rx/rx-elf/rx-elf/rx-elf/lib/64-bit-double\libc.a(lib_a-writer.o): In function `_write_r':
    (.text._write_r+0x14): warning: _write is not implemented and will always fail
    Binary sketch size: 32,868 bytes (of a 458,752 byte maximum) - 7% used
    Minimum Memory usage: 7,613 bytes (of a 98,304 byte maximum) - 7% used
    ..........................
    GR-SAKURA is not found.

    I have a Windows 10 OS and mi IDE is version 1.10

    Thanks

     

    Michael

  • Hi,

    Did you push reset button(red)?
    GR-SAKURA could be showed as USB storage.
    Then GR-SAKURA could be found.
  • Hello Okamiya-san, thanks for reply.
    Yes i pushed the reset button, the PC recognize it as a USB storage. I also tried with web compiler and did all the process (download bin file and put it in), works fine. This trouble just happens when I use the IDE.
    I want to write code offline... Is there any way to retrieve the .bin file from IDE?
    Thanks again

    Regards,

    Michael
  • Hi Mike,

    As you might know, when IDE flash .bin to GR-SAKURA, it calls "SaveSketch.bat", and then "CheckVolume.bat" is also called to check if drives "A" to "Z" exist.
    For example in my enviroment, GR-SAKURA is recognized D drive. When I call "CheckVolume A GR-SAKURA" in DOS at \ide4gr-1.10\hardware\tools\rx, DOS returns error. But When I call "CheckVolume D GR-SAKURA", DOS returns no error, then "SaveSketch.bat" copy .bin to GR-SAKURA correctly.

    What drive is your GR-SAKURA recognized ?
    Could you try "CheckVolume (Drive) GR-SAKURA" at \ide4gr-1.10\hardware\tools\rx as administrator ?
  • Hi Mike,

    Let me say one thing. When you set check for "compilation" to show verbose output,

    You can open the folder where .bin file output by copying the pass shown in the console as below.

     

    When you couldn't solve, please try the above though it's a bit troublesome.