GR-KURUMI Introduction by GR-SAKURA Admin
This is a Japanese Rulz translation contents
Outline
Top Back
GR-KURUMI is a GR reference board, the 2nd in the Gadget Renesas Project. Compatible with Arduino Pro Mini, GR-KURUMI hardware (external board dimensions, external pin layout) and software both supports Arduino language and standard libraries. Therefore your existing sample codes written for Arduino can be used as is.
The following features are unique to GR-KURUMI and not available on Arduino Pro Mini. These features are perfect for creating small, low-power gadgets!
Specification
Creating Sketches
Basically, the Renesas Web Compiler is used to create sketches but e2studio and CubeSuite+ can also be used as a local environment.
The RLduino78 library cannot be used to develop Arduino sketches in combination with CubeSuite+, as the library was created with the GNU compiler GNURL78.
Web Compiler login: http://japan.renesas.com/products/promotion/gr/index.jsp
When using e2studio: http://japan.renesasrulz.com/gr_user_forum_japanese/m/mediagallery/139.aspx
Programming a sketch in GR-Kurumi
Unlike GR-SAKURA, GR-KURUMI cannot be programmed like a USB memory. Just as with the Arduino Pro Mini, your sketch is programmed using a module manufactured by FTDI that includes a USB-to-serial conversion IC. The photo shows the connection between GR-KURUMI and the USB-to-serial module. Kurumi Writer is provided as the dedicated programming software for GR-KURUMI. It can be downloaded as a file from the project created with the Web Compiler. Both Windows and Mac versions of Kurumi Writer are available.
FTDI modules that have been tested with GR-KURUMI:
Hardware Information
Software Information
Contributors Comments
Suzuki
We outlined all the GR-KURUMI information here as it was difficult to figure out whether info was related to GR-SAKURA or GR-KURUMI!
R_e19
KURUMI debut!
Congrats on the debut! I hope you have fun with KURUMI.
@chobichan
Can I use, for example, a 20-pin type G13 when developing a program for KURUMI-chan with the Web compiler?
You should be able to. According to the device UM, the functions are the same for 20 pins and 48 pins. And, sorry for the slow-as-a-turtle response!
No worries! BTW, Akizuki seems to be handling IC lead frames these days.akizukidenshi.com/.../gC-07064It got me imagining a narrow dip 28-pin Kurumi-chan!
Darn, and I was just at Akizuki yesterday. I need to go buy one!