V850ES_JG2_μPD70F3718

I must work with a old project and board (I don’t know it) with microprocessor V850ES_JG2_μPD70F3718. I need debug the system.

How?

I installed with Cubesuite v1.40, after the installation I clicked on “Project” -> “Create new project” 

When i click on "create" i get:

I checked on the folder and i understood the files "uPD70F3718_common.xml" and "DF3718.800" are missing.

Anyone can help me for download this files or every other kind of solution?