E8A

I am wondering if there is any possibility to repair faulty E8a devices

 

I have already three dead ones despite using external power supply

 

Thks in advance,

 

Jean-Pierre

Parents Reply
  • Here are the resuls for the 3 E8A:

    The first is totally dead, no hope to make it work again

    The second is working from time to time, very strange behaviour...

    The third is working fine but when using 'program flash' option to connect to the target system,
    the following error message is displayed after building all files:
    'Flash memory writing NG.
    Written data are not identical with the program data'

    Surprisingly the target is system is working fine despite this error message

    Thks for your usual support
Children