R5F6411FNLG programming help needed

Dear friends , hello to all :)

i need your knowledge about R5F6411FNLG processor.

My problem is my cameras firmware update failed and i bricked a lens olympus 12mm

and olympus software not dedects lens no more and no way to use olympus software.

i checked inside mcu is R5F6411FNLG , i have segger jtag but this mcu is not in list.

camera pinout is attached and i have firmware file.

How can i programme this file to my lens back? OL103011.rar

Parents Reply
  • Sorry, I cannot answer the question about the programming software as I (a) am not sure which software you use and (b) don't know your memory dump.
    I assume you mean FDT software. The message window should say which memory areas have been read like this:
    FCF Settings Applied: R5F64535, (C:\Tool\Renesas\FDT4.09\kernels\ProtD\R5F64535\Renesas\1_0_00\)
    This kernel will set the E2 Data Flash as ECC OFF
    Opening file Z:\_SharedDirectory\WorkSpace\FDT\1MB_FFF00000.mot
    File loaded: 0xFFF00000 -> 0xFFFFFFFF [User Flash]
    File loaded: 0x00060000 -> 0x00061FFF [Data Flash]
    File loaded: 0x00062000 -> 0x00063FFF [E2 Data Flash]
    ID Code = 0xC3 0x46 0x0F 0x85 0x70 0xF4 0x4E
Children