Hello friends
im trying to prog r5f6411flng with usb-rs232 converter(in pictures i added) and renesas programming software.
i find all pinouts and i tried to make all connections up to datasheet, but im not still succesfull.
i made all connections as datasheet
i used 2.2k ohm to vcc to power nmi , cnvss,ce.because i coudnt find any value at datasheet
device originally powered with 3.3v also u tried 5v to. when i applied 5v nmi , cnvss, ,ce voltage changed to3.3 volt.
where i am making wrong?
VCC is 3.3
and i measured while connected to programmer
SCLK= GND
NMI=2V
CNVSS-2V
RESET- NOT CONNECTED (I CUT LINE AT PBC)
EPM-GND
CE-2V
Dear frank ,
Thank you for answer all the time.
But im very curious about when u will start to tell me what l have to do.because always I'm reading what I cant.
I clearly said I'm not good at this processor.im always working on Motorola, nec , atmega with special programmers as upa , xprog etc etc With schematic.
For long time I'm trying to find what I have to do , because I have several more projects about automobiles , but I und there is not enough support about renesas products.
I'm really upset about to listen what I cant.
I hope u decide to tell me what I have to do.
Best regards
Cagatay erdilmen