Hi!
I am currently developing an electronic board using the microprocessor R32C/118.
For the connection of debuger E8a I found two different types of connections:
and provides a connection by pins P64, P65, P66, P67, P55, P50, CNVss,RESET #
this one provides a connection by pins P29, P30, P31, P32, P39, P44, CNVss,RESET #
My question:
I would like to know which of these connections is good, and if both are possible, what are the features not available while debugging, in the case of using one or the other connection (memory expansion, UART1 ...).
Thank you in advance for attention you pay to my question.
Where do you see that the RSK uses P29 and so on? That's not true.
The RSK uses P64-P67 and P50/P55 as is mentioned in the E8a manual.