Hi Frens,
I am still trying to perform the flash write and erase in R32C153 controller.
I learned from the forum that the E8a debugger should be in Debugging of CPU rewrite mode to do so.
But when i use this option these message pops up..
Fatal error: Unknown exception in driver (#E11)
Please help me to correct this .. I have also tried the other options of E8a debugger, but the the flash erase and write are not working.. There are no errors.
Thanks
Anikesh
Thank you