I have been experiencing continually resets after i download my program and run. This is a new issue, as i have been able to use the emulator for ~2 months without any problems. I have confirmed this issue on two separate units. I am able to connect to my device(s) and download my program, the issue occurs when I run (select "GO") my program. It will reset over and over and HEW says it loses communication.
Things I've tried:
I have ordered a replacement 50 ohm coaxial cable to see if that resolves the issue. Any other suggestions? Has this happened to anyone else?
Note: I am able to load the same image via the FDT tool and it works fine.
So from what I can gather,
Debugger is disconnecting, but the device can run in stand-alone mode without any problems.
A couple of questions then:
Is the right device selected in the debugger settings?
Does your application have a watchdog timer?
Are you using a software reset?
Is the right device selected in the debugger settings? Yes. The settings have not been changed.
Does your application have a watchdog timer? Yes.
Are you using a software reset? Can you elaborate?