I have been experiencing continually resets after i download my program and run. This is a new issue, as i have been able to use the emulator for ~2 months without any problems. I have confirmed this issue on two separate units. I am able to connect to my device(s) and download my program, the issue occurs when I run (select "GO") my program. It will reset over and over and HEW says it loses communication.
Things I've tried:
I have ordered a replacement 50 ohm coaxial cable to see if that resolves the issue. Any other suggestions? Has this happened to anyone else?
I submitted a ticket last week with not much traction...
Thanks for the help, hopefully it will get resolved. For now i just disabled the WDT in my code and it's working.