Hy everybody,
I am using a R2C111 (64pins) for quite a long time and facing today an issue with the Timer A3
I am trying to decrement this timer with a 2 Mhz clock generated from the F2n divider.
It is working fine when the value in TA3 is higher or equal to 10 generating a frequency of 1Mhz
but when setting this value to 5 for instance, the frequency is still at 1Mhz.
Is there a limitation which prevent from generating more then 1 Mhz with the timers?
Thks for your usual help,
Jean-Pierre