R32C (152 GROUP) R5F64525 connection issue

Hello, i have R5F64525 connection using E8a issue. By mistake i wrote into 525 Flash, Data Flash and EE from R5f64524 processor and rewrite Boot sector as well. Now im trying to establish connection with 525 processor using E8a to write back files from 525 processor, I'm using Flash Development Toolkit 4.09 software. I can make connection with other 525 processors which are intact. Comunication is Via P6_4/P6_5/P6_6/P6_7. Any advise on how to make connection with chip