Hello,
Is the clock recovery PLL MK1575 temperature stable? If not, could you provide data of its temperature stability?
Regards,
Jakub
Hi Jakub,
Since this device is originally from IDT, I'm not really sure if Technical Support have the data about its performance with respect to temperature. But, yeah feel free to submit a ticket to Renesas…
I don't think we that data here. However, I do believe that as long as you operate within the recommended operating temperature, the device would operate normally.
JBRenesasRulz Forum Moderator
https://renesasrulz.com/https://academy.renesas.com/https://en-us.knowledgebase.renesas.com/
Since this device is originally from IDT, I'm not really sure if Technical Support have the data about its performance with respect to temperature. But, yeah feel free to submit a ticket to Renesas Technical Support. Hopefully they have the data that you need.
Regarding your question, the recommended operating temperature specified in the datasheet refers to ambient temperature. So I do believe that as long as you operate with the temperature range, performance of the device will be stable. But ideally, you should operate at room temperature of maybe 20°C to 40°C as much as possible to avoid performance issues due to temperature.