This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

A question about the 853S011BMILF interface and termination

Hi Support Team! 

Just a question about the 853S011BMILF device.  This is a distribution/buffer chip meant to interface to other PECL devices.  This device is going to be used as a distribution IC for clocking the AD9251 (ADI 14 bit ADC).  The source oscillator also has a PECL output.  The datasheet for the AD9251 is linked here (see page 25, Fig 52):

https://www.analog.com/media/en/technical-documentation/data-sheets/AD9251.pdf

This shows that in their scheme to use a couple 240 ohm shunt resistors and coupling caps into the ADC inputs.  Would this be acceptable in interfacing the 853S011 with the AD9251?  Typically when interfacing PECL devices I would see either bias resistors or a resistors with an equivalent thevenin source but this is a little different.  Your datasheet calls out what I have typically seen.

I want to trust ADI's datasheet but they probably have not tried every device out there so this is what I am asking here. 

Thank you!




[locked by: Sai (SWF) at 12:50 (GMT 0) on 14 Jun 2022]