ClockMatrix Output Coarse Phase Alignment

Hi,

we want to use the 8a34001 system synchronizer in one of our new products. For evaluation we are experimenting with the evaluation board.

We can configure a lot of our desired settings successfully, but we fail to synchronise the output phase of two outputs derived from the same input clock with different FODs. The coarse phase offset between the two output seems to vary randomly between reconfigurations of the parameters.

Our assumption is that the output divders are not synchronised. But we do not understand what is necessary to do that.

The ultimate goal is to have to identical clocks with 10 MHz each that have a programmable phase offset between them.

Beside a short comment in the Timing Commander I could not find any documentation on how to reset the output dividers simultaneosly. 

Do you have any tips for us how to do it?

We would also be willing to pay for an FAE to train us or provide a configuration to us.

Regards,

Kolja