I have a Versal evaluation board from AMD. The circuit card utilizes the 8A34001. I want to reconfigure clocks. In the documentation for the evaluation board, it is stated that the clock configuration was created with the "ClockMatrix" utility using ClockMatrix_8A340xx_V8.1.0.tcp. Where can I find the utility and the tcp file? I'm searching the Renesas site, buty coming up empty. Thanks
Hello,
Let me see if we can dig up that version. (Internal Reference: TECHSUPP-7613 )
Please see attached.
ClockMatrix_8A340xx_V8.1.0.tcp.zip
The rest is with Timming Commander.