Dear all,
I have a question regarding the LOL signal of the the 8T49N241 frequency translator which can be output via GPIO3. When using the device in synthesis/free-run mode without using the digital PLL, does this signal reflect the lock status of the analog PLL? The datasheet clearly states that the signal reflects the signal of the digital PLL but what confuses me is that for the Xilinx ZCU104 board, the signal is directly routed to the FPGA fabric and used as the "tx_refclk_rdy" signal for the video phy controller. When only using the TX capability, the 8T49N241 device is configured in free-run mode and, according to the datasheet, should therefore not generate a LOL signal.
My second question is about the DBITM setting in register 0x0069. According to the datasheet, this bit should have a default value of 0. In my case, it is 1 after reset. What does this setting (as well as VCOMAN and DBIT) do?
Best regards,
Jelle
Hello Jelle,
I am going to confirm a few things with our engineering team and get back to you. Would you be able to share a part of your schematic that shows this device. ( TECHSUPP-7904 )
Hi Michael,
Thank you for looking into this. Unfortunately, I cannot share the schematic directly since I am using a commercial FMC -> HDMI board but the schematics seem to be based on the ZCU104 design which can be found here: https://docs.amd.com/api/khub/documents/g76en4BfB6qIp2gHDRkQxg/content?Ft-Calling-App=ft%2Fturnkey-portal&Ft-Calling-App-Version=4.3.55#G5.602649 (ZCU104 Board User Guide (UG1267), Figure 3-19).
Can you provided your configuration information, please this will help us determine if there are any possible issues.
If you don't want to provide that publicly you can send me a private message or open a Support Ticket
Hey Michael,
I am happy to share my configuration but I don't see how it is related to my general questions:
- Can the device generate a LOL signal on GPIO3 when in synthesizer mode?
- What are the DBITM, VCOMAN and DBIT settings and what could be the reason for DBITM being '1' after reset despite its default value being '0' according to the datasheet?
Please let me know if you still need my configuration.
Best,
Yes, please do.
this is my configuration:
0A 50 00 60 67 CD 7C 01 03 00 31 00 00 00 00 0000 07 00 00 07 00 00 77 6D 06 00 00 00 00 00 FFFF FF FF 01 3F 00 30 00 08 66 66 00 01 00 00 D008 00 00 00 00 00 08 00 00 04 00 22 22 24 22 0200 02 02 00 02 00 00 0D 02 00 02 02 00 02 02 0002 00 00 02 02 00 02 00 00 00 00 00 00 00 00 0000 00 00 00 00 00 00 A0 89 0F 2B 20 00 00 00 0B04 01 FF FF 01 FF FF 00 00 00 27 00 00 00 00 0000 00 00 00
Jedi,
Can you tell me the exact part number you are using - we are wondering if you are using a (what we call) Dash code. (Example: 8T49N241-998NLGI ) Since these parts can be customized and factory programable.