I have a DEV5L1503 evaluation board which I have assembled. I can't get it to program either the evaluation board or a 5L1503 inserted into the socket. The Timing Command says device not found at any of the selected addresses. The device is OTP and does not have an I2C interface, so it's not clear what this means.
I have tried:
- Different USB ports and computers
- Checked and re-checked the orientation of the IC in the socket
- Jumper JP2 installed and removed
It's not clear to me why this isn't working. Do any of the DIP switches need to be set? The documentation only explains two of them.
All I want is to multiply a 10MHz clock to 25MHz. One of the older parts would be ideal, but unfortunately they are all discontinued.