This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

9BV0641

Hi, 

I am planing to use the 9BV0641 PCI clock fanout to fan out a PCIe 3.0 clock to a packet switch and two PCie 1.0 outputs. I have questions about configuration and start up routine. I can't use the SMBus during start up, other than debugging, I was wondering if this is possible? I read that you can configure the IC through the pins but was not able to understand which pins I should used and how should I set them up. Can you help in this regards? Any documents or reference designs are welcomed. 

Best regards,

Besnik




[locked by: Michael Quirk at 20:15 (GMT 0) on 13 Aug 2024]