Hi,
I am planing to use the 9BV0641 PCI clock fanout to fan out a PCIe 3.0 clock to a packet switch and two PCie 1.0 outputs. I have questions about configuration and start up routine. I can't use the SMBus during start up, other than debugging, I was wondering if this is possible? I read that you can configure the IC through the pins but was not able to understand which pins I should used and how should I set them up. Can you help in this regards? Any documents or reference designs are welcomed.
Best regards,
Besnik