8V97051L V_CP power consumption vs ICP

Hi.


The 8V97051L datasheet specifies 21 mA as typical current consumption for the V_CP rail. This is when ICP is set to 0.31 mA.

How much will V_CP's current consumption increase if ICP is set to 5 mA? I don't need an exact figure but it would help if I knew that it increases by 1, 10 or 100 mA.


Regards

Parents Reply Children
No Data