Hello
I'm new to the 8a34001 and Timing Commander GUI.
I would like to know where I can download the latest tcs file for the 8A34001 so that I can start a new project with Timing Commander.
Thanks a lot
Ben,
From our webpage here is the link: Timing Commander Personality File for ClockMatrix 8A34001 (V10.13.0, FW4.8.8, FW4.9.8)
Thank you Michael.
What is the reason for providing to firmware versions in the personality file ? What's the differences between the two ,
The evaluation board I have already contains the FW4.8.8, do I need to upgrade it for 4.9.8 ?
I have an old project which was done with FW4.8.7 : do I need to downgrade my board to 4.8.7 before applying the config or can I leave it with 4.8.8 ? I'm guessing that there is no pb to leave the current (newer) firmware.
Thank you