how can the data flash be excluded from erase by E2 debugger RL78/G13

Hi

 

having the data flash erased every time i load code complicates my development immensely.

So if there is a way to avoid that i would be super happy.

 

Also if the project  linker settings could have check boxes to create a linker file depending on if eel/fdl/self programming is used or not would save many support questions as the sample linker files are for a single memory size. (and 4 years old not matching)

older tools/different processors had/have a linker file "editor" in eclipse but this seems to be absent for RL78

 

I may have misunderstood a lot as I am new to the scene, but browsing trough the forum this seems to be 2 of the top issues people have, including me.

 

thanks

/nicholas