I have installed the latest e2Studio and FSP (setup_fsp_v4_0_0_e2s_v2022-07.exe) from the Github of Renesas (https://github.com/renesas/fsp/releases/tag/v4.0.0).
Strangely it does not show me any details which I want to edit in the property tab of the 'FSP Visulization' perspective.Details from Help->about e2 studio are as follows version 0200-07 (22.7.0)Build id: R20220704-1123I have no other way to put images so I uploaded it as a video on youtube and put the link herehttps://youtu.be/901qp1aPMaM
You can also use Ctrl + V to paste the image if you can't find the 'Upload' button. But it seems like there is something wrong with your browser. Can you try clearing the cache of your browser…
Hello 444. To access the configuration of FreeRTOS, please create a New Thread from the Stacks configuration screen and then you can access the FreeRTOS properties and settings, which are explained in the FSP…
Please see the issue here, this is the screen recording unloaded https://youtu.be/901qp1aPMaM
Hello 444. To access the configuration of FreeRTOS, please create a New Thread from the Stacks configuration screen and then you can access the FreeRTOS properties and settings, which are explained in the FSP user manual.- JayeshIf this response, or one provided by another user, answers your question, please verify the answer. Thank you!Renesas Engineering Community Moderatorshttps://community.renesas.com/https://academy.renesas.com/en-support.renesas.com/.../
Thanks a lot, Jayesh (SWF) !!!