This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Synergy S5D9 SPI DTC

I'm try to config the SPI DTC, but many parameter was locked, as below, can you help me with this issue?




[locked by: Sai (SWF) at 13:29 (GMT 0) on 5 Jan 2023]

Top Replies

  • Hello . The DTC is already configured with the predefined settings and it will be automatically used for the SPI communication. The parameters with the lock symbol are fixed for SPI communication and…