I'm try to config the SPI DTC, but many parameter was locked, as below, can you help me with this issue?
Hello Jali. The DTC is already configured with the predefined settings and it will be automatically used for the SPI communication. The parameters with the lock symbol are fixed for SPI communication and…
Hello Jali. The DTC is already configured with the predefined settings and it will be automatically used for the SPI communication. The parameters with the lock symbol are fixed for SPI communication and can't be modified. For more details, please check out the following thread: community.renesas.com/.../61181-JayeshIf this response, or one provided by another user, answers your question, please verify the answer. Thank you!Renesas Engineering Community Moderatorshttps://community.renesas.com/https://academy.renesas.com/en-support.renesas.com/.../
Thanks Jayesh, I see.