e-AI translator error on PyTorch model translation

Hi,
I met the eAI-501 error when I followed the guide of "3.5 How to create/save PyTorch model file" in the e-AI Translator V2.3.0 User's Manual.

Following is the log message.

"[2022-11-03 19:13:07,266 ERROR requirements.py:217 - log_exception() ] eAI-501 : Uncaught Exception
An unhandled exception has caused this script to terminate prematurely. Here are the details :

Traceback (most recent call last):

File ".\bin\network_decoder.py", line 143, in <module>

File ".\bin\network_decoder.py", line 112, in generate_network

File ".\bin\error_code.py", line 37, in reraise

File ".\bin\network_decoder.py", line 104, in generate_network

File ".\bin\pytorch_dep\network_decoder_pytorch.py", line 157, in generate_network

ValueError: invalid literal for int() with base 10: ''

[2022-11-03 19:13:07,266 INFO requirements.py:218 - log_exception() ] Translation FAILED!!
[2022-11-03 19:13:07,266 INFO requirements.py:189 - remove_object() ] Uninitializing and cleaning up the translator object.."

I'm not sure what I missed. Could you check this error message and the used file (mnist.py)?

import torch
import torch.nn as nn
import torch.nn.functional as F

class Net(nn.Module):
    def __init__(self):
        super(Net, self).__init__()
        self.conv1 = nn.Conv2d(1, 8, 3, padding=1)
        self.conv2 = nn.Conv2d(8, 16, 3, padding=1)
        self.dropout1 = nn.Dropout(0.25)
        self.dropout2 = nn.Dropout(0.5)
        self.fc1 = nn.Linear(784, 128)
        self.fc2 = nn.Linear(128, 10)

    def forward(self, x):
        x = self.conv1(x)
        x = F.relu(x)
        x = F.max_pool2d(x, 2)
        x = self.conv2(x)
        x = F.relu(x)
        x = F.max_pool2d(x, 2)
        x = self.dropout1(x)
        x = torch.flatten(x, 1)
        x = self.fc1(x)
        x = F.relu(x)
        x = self.dropout2(x)
        x = self.fc2(x)
        output = F.softmax(x, dim=1)
        return output

Hello.
Today, I updated to the latest license file of e-AI translator (License_V230_20221130) according to the guide of 2.2 Copying the License File for the e-AI Translator in the e-AI Translator V2.3.0 User's Manual. After that, the PyTorch model has been successfully translated by the updated e-AI translator.

+---------------------------------+-----------------------+-----------------------+
|        Layer Information        |    Size Information   |   Speed Information   |
+------------------+--------------+-----------+-----------+-----------------------+
| Layer Output No. | Layer Name   | ROM(Byte) | RAM(Byte) | MAC Operations(times) |
+------------------+--------------+-----------+-----------+-----------------------+
|        1         | Input        |         - |     3,136 |                     - |
|                  |              |           |           |                       |
|        2         | Convolution  |       320 |    28,688 |                56,448 |
|                  |              |           |           |                       |
|        3         | ReLU         |         - |    25,088 |                     - |
|                  |              |           |           |                       |
|        4         | Max Pooling  |         - |     6,272 |                     - |
|                  |              |           |           |                       |
|        5         | Convolution  |     4,672 |    20,736 |               225,792 |
|                  |              |           |           |                       |
|        6         | ReLU         |         - |    12,544 |                     - |
|                  |              |           |           |                       |
|        7         | Max Pooling  |         - |     3,136 |                     - |
|                  |              |           |           |                       |
|        8         | Full Connect |   401,920 |       512 |               100,352 |
|                  |              |           |           |                       |
|        9         | ReLU         |         - |       512 |                     - |
|                  |              |           |           |                       |
|        10        | Full Connect |     5,160 |        40 |                 1,280 |
|                  |              |           |           |                       |
|        11        | Softmax      |         - |        40 |                     - |
|                  |              |           |           |                       |
|        12        | Output       |         - |        40 |                     - |
|                  |              |           |           |                       |
+------------------+--------------+-----------+-----------+-----------------------+
|                  |              |           |   100,744 |                       |
|                  | TOTAL        |   412,072 +-----------+               383,872 |
|                  |              |           |    40,808 |                       |
+------------------+--------------+-----------+-----------+-----------------------+

# MAC : Multiply and ACcumulation(Number of product-sum operations)
# Total RAM size (Upper) : Total size of All layers.
# Total RAM size (Lower) : Actual size (Input + dnn_buffer1 + dnn_buffer2 + Output).

B.R.
Y.H.Lee

Parents Reply Children
No Data