My E2 Studio hosted a FSP of edition 4.0, while my BSP supported up to 3.6, how to degrade the FSP in e2 studio, could I add more than one edition in e2 studio?
Is the compilation without errors and not more warnings than in 4.0?Is it loadable to the board?Does it run like expected?
Yes you can, but I would not recommend it. 4.0, 4.1, 4.2 is no problem. Version 3.x and 4.x means a major version (SW) change. I would suggest to install both versions in different locations on your PC. Having your 4.0 project on left and a new 3.6 minimal BSP on the right screen. Double click the configuration.xml on both and open the Stacks tab. Slowly "New stack" on right till you see the same (similar) tree like your working project. e2studio will show you in red if a property value is not correct. Have anybody else a better solution?
I just downloaded a FSP 3.6 and installed it beside 4.0, and I can alter the FSP edition in "Board Support Package Configuration" window. Is that OK?
Hello,
I have a bug. I am not able to Import dialog box in the FSP Packs. FaceTime App
any on help me.
I do not understand your issue. After you install the old FSP version to e.g. C:\Renesas\RA\e2studio_v2022-07_fsp_v4.0.0 you should have in the directory C:\Renesas\RA\e2studio_v2022-07_fsp_v4.0.0\internal\projectgen\ra\packs with both file names:- Renesas.RA.4.0.0.pack- Renesas.RA.3.6.0.pack
Make a backup of your project.
So after you File -> import -> existing project into workspace -> choose directory .... -> you should see configuration.xml -> double click on it -> go to tab BSP and choose the FSP version you want.
Hi Ashley - this is a new issue unrelated to this topic. Please submit a new post and, while doing so, I recommend providing more detail and screenshots to get better responses.
-Josh
If this response, or one provided by another user, answers your question, please verify the answer. Thank you!Renesas Engineering Community Moderatorshttps://community.renesas.com/https://academy.renesas.com/https://en-support.renesas.com/knowledgeBase